LTE TDD

Cell Parameters Uplink (Basic TDD)

For Waveform Playback (ARB) capability.

This topic describes the settings of the Uplink > Cell Parameters node for a Basic TDD carrier.

State

Total Number of Antennas

Antenna Port

PUSCH DFT Swap

State

Turns the uplink transmission off or on.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:UL:STATe <value>

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:UL:STATe?

SCPI Example

RADio:LTETdd:WAVeform:CCARrier:UL:STATe OFF

Notes

None

Dependencies

None

Preset

Off

State Saved

Yes

Initial S/W Revision

A.20.01

Total Number of Antennas

Query only

Displays the total number of antennas.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:UL:APORts:COUNt?

SCPI Example

RADio:LTETdd:WAVeform:CCARrier:UL:APORts:COUNt?

Preset

1

State Saved

Yes

Min

1

Max

4

Initial S/W Revision

A.20.01

Antenna Port

Query only

Displays the antenna port number.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:UL:APORt?

SCPI Example

RADio:LTETdd:WAVeform:CCARrier:UL:APORt?

Preset

0

State Saved

Yes

Min

0

Max

3

Initial S/W Revision

A.20.01

PUSCH DFT Swap

Turns PUSCH DFT Swap on or off.

PUSCH DFT Swap influences how data is mapped to resource elements in the physical uplink shared channel after discrete Fourier transform is performed. PUSCH DFT Swap can be turned on or off to provide two different interpretations of how data should be mapped to resource elements in PUSCH channels.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:UL:PUSCh:DFTSwap ON|OFF|1|0

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<channel>:UL:PUSCh:DFTSwap?

SCPI Example

RADio:LTETdd:WAVeform:CCARrier:UL:PUSCh:DFTSwap OFF

RADio:LTETdd:WAVeform:CCARrier:UL:PUSCh:DFTSwap?

Preset

Off

State Saved

Yes

Initial S/W Revision

A.20.01

Carrier Uplink (Basic TDD)

Welcome to LTE TDD